Hi,hello, can someone tell me how to enable and disable external interrupts on the ST Visual Develop interface. I use the general library. Thanks.And no matter what I do, first the external interrupt routine switches as if it has a priority.
Hello stm community,I am working with the STM8S001J3 processor on the ST Visual Develop Toolchain.And I use the TIM1 and the TIM2.The Tim1 is enabled via the external port when the D port is active. It is used to work synchronously with the 50hz/230v...