User Activity

Hello,I'm going to use the Memory connector CN11 and CN12 on STM32H753I-EVAL to evaluate an external NAND flash memory. According to the reference manual of RM0433 page 838, the Chip Select is NCE, but NCE could not be found on the pin list of CN11 a...
Does someone know where I can find the files of Loader_Src.c and Dev_Inf.c for STM32H753I-Eval?I'm going to use them to develop customized loader for external memory. However the /ExternalLoader directory mentioned by ST-LINK Utility Software Descrip...
Hi,I'm looking for the files of Loader_Src.c and Dev_Inf.c for STM32 ST-LINK utility external loader developing. Can someone tell me where these files are located? The user manual of UM0892 says "They are in an external loader project", but I don't k...
Hi,I tried to use ST-LINK_CLI (v3.5.0.0) for STM32 ST-LINK Utility (v4.5.0.0) on Win 10, and found issue of it. When entering any command on ST-LINK_CLI prompt, the prompt closed immediately, I could not see any result about the command I just keyed ...
Hello,Can someone let me know how to bring STM32H753XI-E02 Eval board back to its original status (i.e. factory default)?I tried to implement Quad SPI application and found the Eval board did not work well. The USB port (CN23) did not communicate and...