Posted on June 08, 2018 at 14:40 Hello everyone, I have 9 pins of ADC that each of them will received signal from function generator 20 kHz. I want to use ADC to store the data inside an array by using DMA2. ADC1 has 3 pins, ADC2 has 3 pins, ADC3...
Posted on January 28, 2018 at 17:21Hello everyone,I apologize if my question is too basic for this forum but i've been reading so many sources in the internet and i am still confused and I am pretty much new in this subject.I want to hear ultrasound...
Posted on June 11, 2018 at 16:14 Hi, I've tried with constant voltage and it works fine, with the configuration both for triple mode and independent mode. I haven't try to do triple mode for one ADC and 9 channels. I will check it out. I have...
Posted on June 11, 2018 at 14:03Hi,I tried increasing the sampling time from 15 to 28 cycles but the result is still not what i want. The input is sinusoid and i expect the ADC output will look like sinusoid also as the sampling is very fast. The ou...
Posted on June 11, 2018 at 11:50Hi,Because my input is 20 kHz, and want to set timer for sampling 200 kHz, so samplingtime+converstiontime+intersamplingdelay < 5 us , right?The conversion time is (samplingtime+resolution)=15+12=27 cycle ...