I would like to compare a lot of CNN models in terms of RAM usage.If I analyze a single model the important result I am interested in is the ram (total) usage. As that practically defines, if the model fits into the RAM. weights (ro) : 1,544 ...
I am using a Nucleo-F676ZI and trying to run a dnn on the mcu. I can run the NN using the "application template" but I want to use the "validate on target" in order to obtain runtime without developing the data transfer from the host system to the mc...
> You can also try to select "Validation" as the application (and not template), and let X-CUBE-AI configure automatically the USART for you.How can I set "validation" as the application?I did only find how to set it in the selection of the x-cube-ai...
Thanks for the reply!I did test both solutions. Unfortunately, both did not work. Furthermore, I did test other x-cube-ai releases.It is possible to use the COM port that is directly connected to the ST-Link correct? (USART 3)Is there any way to get ...