User Activity

Hi,I have a scroll list that works perfekt in the simulator, but when running it on target (STM32H735) I need to set a periodic update of scollList.invalidate(), to get it to work. The problem is that only the first and last element show as selected,...
Hi, how exactly is the cortex_m7/gcc/libtouchgfx-float-abi-hard.a built (i.e compile and link options)?For example if a make a object dump on the lib I get:touchgfx::muldiv(long, long, long)But the header file use int32_t instead of long and that giv...
I use this code to switch to bank2 after downloaded fw image in bank2. I have verified that the first address is (stack pointer) is pointing to the SRAM. But still it starts the code in bank1.Is there any example that I can follow?       /* Unlock op...
Kudos from
Kudos given to