User Activity

Hi to all.I'm starting a new project where we use the STM32H7S3V8H, and with the code generated with the STM32CubeMX (see IOC file attached) it compiles perfectly the Boot code but the Application code allways fail with the following error message:"c...
Hello I am developing on the NUCLEO-H563ZI board a system in which I need to obtain an IP address via DHCP.I have implemented the client following the guidelines of the documentation provided by ST as well as THREADX and NETXDUO and, I have strange b...
Posted on September 20, 2017 at 12:35Hi guys.I'm working in a STM32L476JGY based project using the board STEVAL-STLCS02V1.The code generated by the Cube using the default clock configuration 'forgets' initialize the M value of the PLL struct, see or...
Kudos from
Kudos given to