cmu.1
Associate II
since
2022-08-30
2023-06-14
User statistics
6
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About cmu.1
Options
Report User
User Activity
Posts
Replies
example program (TypeV_SetAreaProtection) of ST25R3911B to set ST25TV02K gives error 5
2022-10-12
When using the example program (TypeV_SetAreaProtection) of ST25R3911B to set ST25TV02K, the following error occurred.Code:static void demoNfcv( rfalNfcvListenDevice *nfcvDev ) { ReturnCode err; uint8_t regNum = 0x05; uint8_t...
Re: example program (TypeV_SetAreaProtection) of ST25R3911B to set ST25TV02K gives error 5
2022-10-14
thanks, but the error code is still 5。static void demoNfcv( rfalNfcvListenDevice *nfcvDev ){ ReturnCode err; uint8_t regNum = 0x05; uint8_t regVal; uint8_t endval; uint8_t * uid; //int8_t pwdNum=0; //Pass...
Re: example program (TypeV_SetAreaProtection) of ST25R3911B to set ST25TV02K gives error 5
2022-10-14
ST25PC-NFC software can help me to confirmation �?Password configuration is (00,00,00,00)“
Re: example program (TypeV_SetAreaProtection) of ST25R3911B to set ST25TV02K gives error 5
2022-10-14
After tracking, the screenshot is as follows
Re: example program (TypeV_SetAreaProtection) of ST25R3911B to set ST25TV02K gives error 5
2022-10-14
Thanks, the problem still exists, and the output error message is the same。
Re: example program (TypeV_SetAreaProtection) of ST25R3911B to set ST25TV02K gives error 5
2022-10-12
zone 1 password is (00, 00, 00, 00, 00, 00, 00,00) --8 bytes