Posted on November 24, 2017 at 06:46Hi Yoann,I did a little more digging by reading the WIND messages coming over UART from the SPWF01SA. I see that the board in which the issue is present, I donot see +WIND:32:WiFi Hardware Started message.But in t...
Posted on November 05, 2017 at 08:52Same here... Changing the X-NUCLEO-IDW01M1 solved the problem.. I need to now check what is the issue with the old board. I did tap the uart lines and check in the oscilloscope but I could not see any data transm...
Posted on October 25, 2017 at 15:35Hi,i am facing the same issue. I am using Nucleo-F401REI am using the package en.x-cube-wifi1_firmware_v3.0.2My software was running properly, and I was able to connect to a remote server and trasmit some data over...