Requirments-LCM->1024x600 TFT With CTP and Or 1028x 800 LVDS TFT With CTPColor Depth-> 24bppFPS-> ~30MCU-> _________?RAM-> __________?QSPI-> __________?I have Selected the following Hardware But need expert opinion on this subjectMy Selection-MCU->ST...
We have a dial gauge in the center of the screen and are getting stretched-out images of the dial, What is the solution to keep it in 1:1 ratio?MCU-STM32F750TFT-50 PIN 800X480BIT DEPTH-16BITIDE-STM32CUBEIDE
I have added a Touch screen library and I am unable to integrate it into Touchgfx Project that is opened inside Stm32IDE -I am getting File not found errorWhat I have done so far-Added the file using Properties ->c/c++ general-> path and symbols ->In...
I.want to know the use of series resistance that is placed with STM32H750B-DK and External RAM , And also.with it's Dual Quad SPI interface.Is it possible to leave them as it is or it is compulsory to implement.
So I got the following Calculation:-Screen Resolution- 1280 x 800Color Depth-24 BppFramebuffer = (Resolution L * Resolution W * Color Depth)/8=3,072,000 Bytes or 3.072 MB For 1024 x600 TFTScreen Resolution- 1024 x 600Color Depth-24 BppFramebuffer = (...
Thanks for the suggestions , As you specified in the 3rd bullet point that " In that case, you will either need a 32BITS SDRAM or a screen with embedded memory.If you are using a complex GUI with a high-resolution screen, a MCU with internal flash is...
Thank you @STOne-32 @Tesla DeLorean @CBerg @David Littell For your input, I would just want to clear that Series resistance will be put on the receiver end Right?