Posted on August 24, 2017 at 09:47HiWe have a device which is an USB powered(USB2.0), and on the same USB port is the communication with the PC.So it is powered from the PC.For the ESD protection of the USB lines we add the USBLC6-2SC.Our processor ...