User Activity

I am confused with the SPI operation particularly the raising CS after each byte (which isn't shown in the data sheet figures). I can get the motor to work, but as an example this is what I have to do to send a simple move command. The data is (in he...
This is driving me crazy. First time with this processor. I have AFR2 and NAFR2 set properly for AIN2 operation. I can verify that in the watch window and the disassembly window looks like it is working as expected. If I change the channel to AIN7 I ...
Posted on July 28, 2017 at 19:23Is there a recommended pad layout for the POWERSO36 package? Ap note AN668 regarding this package has a detailed layout for the POWERSO20 package with measurement data, but not the POWERSO36.