Posted on September 28, 2017 at 09:02Hi Peter, the first device (no float VDD pin) has p/n WE 824011; the second with declared VDD pin float capability has p/n WE 824014 (it has 4 I/O channels but I use only 2). The VDD pin capability isn't declared...
Posted on September 26, 2017 at 07:44Hi Peter,I found the same problem and I applied the solution that you wrote.Anyway, I did do some investigations and I found that the extra current draw is due to the TVS USB protection ( a bridge diode plus a ze...
Posted on August 28, 2017 at 12:24Hi,I have the same problem but with STM32L432 device that has not VDDUSB pin, so I can't disconnecting this voltage that is wire connected (inside the component) to VDD. If you or anyone have a suggestion is very ap...