KUMAR SAURABH
Associate II
since
2018-07-19
2023-06-14
User statistics
8
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About KUMAR SAURABH
Options
Report User
User Activity
Posts
Replies
My EEPROM is write protected. How can i disable the password that has been implemented before?
2017-09-26
Posted on September 27, 2017 at 07:16My EEPROM is write protected. How can i disable the password that has been implemented before?
How can I make my M24SR EEPROM Read /Write Password Protected?
2017-09-20
Posted on September 20, 2017 at 12:15How can I make my M24SR EEPROM Read /Write Password Protected?
when should I use NDEF_writeNDEF() and TT4_WriteURI()? Also, If I want to send non URL NDEF messages through NFC, which API should I use in the example NFC code and what are the changes in the code I should keep in mind?
2017-08-08
Posted on August 08, 2017 at 14:39M24SR Cube Expansion example code
Can you provide a circuit diagram for inductor type antenna that is compatible with M24SR?
2017-07-17
Posted on July 17, 2017 at 15:43Can you provide a circuit diagram for inductor type antenna that is compatible with M24SR?
Can M24SR be used for Industrial purposes?
2017-07-17
Posted on July 17, 2017 at 15:41Can M24SR be used for Industrial purposes?
Re: My EEPROM is write protected. How can i disable the password that has been implemented before?
2017-10-05
Posted on October 05, 2017 at 11:30I have forgot the 'write password' that i had used before. How can i disable or recover the password? Also, Is there is process to do hard reset in M24SR?
Re: My EEPROM is write protected. How can i disable the password that has been implemented before?
2017-09-28
Posted on September 28, 2017 at 11:48It's M24SR
Re: Can M24SR be used for Industrial purposes?
2017-07-25
Posted on July 25, 2017 at 12:07Need the info urgently. Please help.