User Activity

Posted on June 29, 2017 at 14:30I try to make some noise using a small 8 OHm @ 1 kHz Buzzer connected to the STM32F446 DAC_OUT1. Seams the PA4 pin got damaged due to high or reverse voltage induced by the buzzer. I used th push/pull GPIO config. Is ...
Posted on June 29, 2017 at 11:58Hi,Im trying to optimize LowPower current consumption of a custom board my hardware guys have made arround a 100pin LQFP STM32F446VET. Currently I fight to find the source of a faulty voltage at GPIO PA4 (Pin 29 with ...