Posted on July 11, 2017 at 15:36Thanks Marsh.nick for providing the example code. It seems the hardware I have has some issues as it is not behaving normally. I will try to confirm that by using another hardware and see if I my code works on that.
Posted on July 07, 2017 at 14:59I have the PCAN USB connected, so that I can transmit and receive the packets from my PC. I have made sure the pins are mapped properly but it gives me the time out error in checking the CAN MASTER STATUS REGISTER BI...
Posted on July 05, 2017 at 21:39Hi ,I am trying to run the CAN example on Nucleo-64 board (STM32F072). If I compile and download the project in processor, the program goes in the HAL_ERROR state and hangs up. I am new to CAN communication, and I hav...