User Activity

Hello,I am attempting to write a first stage bootloader that will load a second stage from SD card into RAM and then jump to this application.The program works when I load the second stage to flash and jump to it and when I run it in RAM with the Deb...
I have inherited a GUI project that has a memory leak which I tracked down to the use of the LISTBOX.If I remove the LISTBOX the memory usage never rises however if I utilize a LISTBOX even if empty memory used by STemWIN will rise until it runs out ...
Kudos from