1) CC1 and CC2 connections from microcontroller are properly connected to TCPP01-M12. 2) When TCPP01-M12 is separately powered up, input given to CC1 and CC2 appears on CC1_C & CC2_C3) When input to CC1 and CC2 are given from the controller, the volt...