No. Unfortunately anything that was suggested did not help. My view was the update to the onboard STI Link got corrupted by the update STI provided and they refused to replace it. I can use the STI-Link from another board to program the microprocesso...
Unfortunately the new IDE version also fails. I see the ST-LINK update facility within this new version of the IDE has also been updated but I get the same error with it nor recognizing the current firmware on the board.Michael
I am using a very short USB cable plugged directly into the front of my machine and I have tested with another STM32 Discovery Board and everything works with STM32CubeIDE and STM32CubeProgrammer. Using this cable I can connect to a serial connectio...
I did use STMCubeProgrammer originally when the upgrade failed and started all this, version 2.10.0. I then tried version 2.8.0 but it also fails to connect. I then was grasping at straws and used the old standalone STLink upgrade utility to see i...
I understand that the firmware version is strange and that is probably why the ST-Link utility won't upgrade the board because it doesn't understand it either. Is there a way around that? This is an official Nucleo-64 board I purchased from Mouser ...