User Activity

Hi,We have come across a bug in the code generated if you use FreeRTOS in STATIC memory mode (rather than the default dynamic mode) , with FatFs. (All generated from the CubeMX).When we run the code we get two CONFIG ASSERTS in the RTOS and it is due...
Posted on June 05, 2017 at 12:57Hi,The following is based on an STM32F401 Nucleo and the IKSA101 Sensor board.  The HAL function was form anearlier version of HAL but matches that in release 1.16.0We have been working with the I2C bus on the STM32F4...
Kudos from