@Eleon BORLINIThanks for your comment. Yes , you have got it correct. X axis is Voltage and Y is millisecond. Red line is INT1 and Blue Line is Voltage for Hardware which i have connected to AIS2DW12 . My expectation and aim was after wake-up duratio...
Hi @Eleon BORLINI ,for better understanding I can share two pictures from Scope. If the Motion sensor power supply is 1.8 V there is no ramp and INT1 works clean. If i set power supply to 3.0 V then i see the ramp. Here is also my configuration for ...