Can I use the Wfe().and create a timer that triggers a event, if so how should it be done?I have a lot of interrupts that are triggered. that disturb my sleep mode.Best regards...PS: I have to sleep every 30 ms and then wake up again
in the user manual: Seconds interrupt, for generating a periodic interrupt signal with a programmable. but it is not as it is with the RTC alarmBest Regards Kadir
Thank you Danish for the fast feedback.The count should run all the time, i.e. switch off every 30 ms, then start again after 30 ms.This is for a low power energy model and something is done every 30 ms. do you think this is feasible?Best Regards Kad...