Per Screenshot 2023-07-21 223418N.png the message is "No I2C Acknowledge from device 0x28 on bus 1."It means that the device was not detected.Possible causes can beHW connection is not correct. -> Check SCL, SDA, and GND wires.The used STM32F072 firm...
Do you mean in host uC to read M2SP's flash thru ACI? There would be no such stack library ACI to pass some flash data.The simplest workaround is to program the data (MAC address in this case) in the flash on host uC, then in the application read the...
50: marking area -- here it means the version of fixed output 5.0 V, so this shall be correct device3: the last digit of the assembly year06: the assembly week