Documentation really says that pullup resistance on NRST is not required but I decided to leave possibility to solder it. I checked board with external pullup and without, it does not make any changes, MCU is still not working correctly.AN2586 only r...
VDD is stable, it has 3.3 V with small pulsations about 5 mV, so it seems that the problem isn't related with power supply. 1V on NRST is not static, but it is not oscillating too. The voltage is floating randomly from 0.4 V to 2 V, but mostly is sta...