User Activity

Hi,I use a X-NUCLEO-NFC06A1shield and a Nucleo-476RG to read a NFC chips ( M24LR64D-W or M24LR04).For my test I use the demo program from ST provided with the shield.I want to read 32 blocks (a block is 4 bytes) with the function rfalNfcvPollerReadMu...
I'm looking for v4.2.0 because the release v4.4.0.0 crashes when I do a "save as" on my board Nucleo-L476RG.
Posted on May 20, 2017 at 15:56Hi,After generation of code with STM32CubeMx (release 4.21.0), Error_Handler() interface present in main.h is not specified to be used in C-style linkage as it's done in the rest of the code.This performing a linkage e...