Hi Osman,I have the same problem changing my project from 4.20 to 4.22, because I am also interested in the new image compression. It would be great to get an information when this bug is fixed or a workaround is known.Thanks for a while.
Hi,I have installed TouchGFX 4.22 and I have the same problem.When I move a copy of the "touchgfx" folder into the directory ".....\Middlewares\ST\TouchGFX" at the moment when the directory is renamed to "touchgfx_backup", my project is completely bu...
Hi, I've got the same problem. I'm working with 4.19.0 and for me it is absolutely necessary to see in the designer what I'll get in the application. Otherwise it takes too much time to "play" with the line spacing until I get a suitable result. I've...