I am checking signal status also for Big obstacle it showing Distance up to 2.1 meter(210Cm) and status is 0, and for small obstacle showing distance up to 1.2 meter(120 cm) and status is zero, it is not useful in outdoor environment , and it Hangs a...
I checked Range status initially it is returning 0, and after that it continuously it is sending 255 , I am using Spark fun VL53L1X sensor and i am working on 8 sensors ,it is working fine if obstacle is there between 4 meter range, if obstacle i...
I am using VL53L1X , code works fine when there is obstacle in the range of 0 to 4 meter ,if no obstacle above 4 meter sensor is giving random values , how we can fix this issue?