Posted on January 10, 2013 at 11:33The exposed pad of the STM8AF6266 VQFN32 package should be connected to Ground. It doesntt prevent to connect the VSS pins. The documents are going to be updated #hardware-qfn32
Hello Jan, I take good note of your comments. Particularly the Analog portion regarding DAC and Comparators. The analog IPs are generally costly in size and we have chosen to remove them knowing the bridge we are offering with the STM32G0 in which y...
HelloFirst thing is your MCU selection. It is going to depend on the nature of your project Automotive (STM8AF/AL)- NonAutomotive (STM8S/L)Mainstream or Low power (STM8S or STM8L)Then I suggest you to start with STM8CubeMX and select the appropriate...
Posted on April 21, 2017 at 17:04Hi,The mission profiles of our STM8 and STM32 families are not aligned with Aerospace requirements. As a matter of fact we are mainly offering products to consumer, industrial, and some STM8 for Automotive markets. B...
Posted on February 06, 2017 at 11:51Hello, let me bring a little precision here. The STM8 is not based on ARM core. This is a proprietary core developed by ST. If the STMAL318AT is not described properly (Something I will check and ask for correcti...