User Activity

The STM32 IDE project shows some "default" mapping to use in the U[S]ART1-6. For example, UART1 has PA9(TX) and PA10(RX). Are these GPIO pins fixed? Can any be used? Is there any restriction on which pin can be used with which UART block?In particula...
Posted on April 22, 2017 at 18:52Hi all,At my company we have an STM32F407 MCU and we are trying to use the in-built boot-loader. I have read  - AN2606 - STM32 microcontroller system memory boot mode and - AN3154 - CAN protocol used in the STM32 bo...