User Activity

Hello GuysI'm using a157-EV1 board and my custom board.Both board have sd card slot and emmc. And possible of linux install to sd card and emmc.Anyway if built images using STM32_Programmer_CLI in Ubuntu environment can be install on the board accord...
Hello​I am using Distribution Package and st-image-core.I had to use sftp while testing my board, so I tried it, but it doesn't seem to be installed in the default package.So, after adding the following to st-image-core.bb, I tried bitbake, but an er...
Hello guys.I have configured ethernet on STM32MP157F using Microchip's LAN8720AI-CP.I base my image on st-image-core of Distribution Package. And dts is configured using CubeMX(meta-st-stm32mp-addons).Currently, it appears as if ethernet is connected...
Hello Guys​Like the subject, I want change the interface RGMII to RMII using CubeMX.(RealTek-RTL8211EG-VB-CG => Microchip - LAN8720AI-CP)Based on STM32MP157C-EV1 Code in CubeMX, I changed the Ethernet option from RGMII to RMII as shown in the picture...
Hello Guys.I have tried bitbake(st-image-core) after a long time.But I can't proceed with the following error.This error is partial, and many of the same errors appear(Attach the error as text).I don't know how to fix it. I need help.can't find file ...