User Activity

To understand capacitive touch / TSC library based application, I’ve been studying the polling based sample code given in AN5105 for STM32F072B-Disco evaluation board. After tweaking the code to customize for the application, I’ve a few questions as ...
Which evaluation board I can use to practice and develop code on Capacitive Touch Sensing, which is suitable with STM32F302R8?I have STM32F302 Nucleo board with STM32F302R8 MCU, which supports touch sensing. I need to learn and develop a practice cod...
Hello,I need to be able to generate a center aligned PWM signal on two Ch. with 1.5MHz PWM frequency. The duty cycle variation will have dead time inserted in it. In order to generate 1.5MHz for center aligned signals, I need to calculate ARR Registe...
Kudos from