User Activity

Posted on December 01, 2017 at 21:47Has anyone used the IHM02A1 and got either the project files or the pre-compiled binary and hex files to work? If so, could you please tell me if you did anything to get them to work or did they simply work out of...
Posted on November 30, 2017 at 23:43I am using a X-NUCLEO-IHM02A1 dual stepper motor driver evaluation board paired with a NUCLEO STM32F302R8 board. My IDE is the System Work Bench for STM32. The motor driver comes with a software package for contai...
Posted on August 25, 2017 at 21:00I am building a project that I've previously built with success, but am now getting the error Conflicting Types for 'HAL_Init'. Since my last build, I've only made small changes to the code for my timers and have no...
Posted on June 26, 2017 at 04:33I need help with the integrated CANBus controller on the NUCLEO STM32F302R8. We are using STM32CubeMX to generate our setup code with the  STM32Cube_FW_F3_V1.8.0v Firmware package provided by ST. We are then using the...