Posted on October 28, 2017 at 20:27Hello,Yo can simply enable CCR interrupt in one pulse Timer. In the corresponding CallBack you increment a variable. This variable will show you how much the Timer output state has changed.
Posted on October 26, 2017 at 12:33Hello ,You can generate one signal and measure another with the same timer but with limitations. Let's talk about TIM4 for example. It has 4 independant channels but all the channels have only one counter and one A...
Posted on October 26, 2017 at 12:09 Hello de_Miguel.Endika, I have a very simple way to do it I wrote an article about measuring high frequency signals with a good precision. To do that, I simply used a second Timer to divise the high frequency...
Posted on June 04, 2017 at 16:35 Hello Gibiino.Vincenzo! What you said about he transistors is totally true ! Concerning the capacitors you can do it without hem but I don't advise you do remove them because they're useful fore high frequency ...
Posted on June 01, 2017 at 04:16you can generate phase-shifted PWM signals with 2 different ways :1) You can use the feature : Output toggle which can generate up to 4 phase-shifted PWM signals with controlled shift but all signals have the same dut...