User Activity

Using the MCSDK 5.0.1, I can startup and when I get to 2000 rpm I get Start-up failure I've tried adjusting several parameters in Workbench's 'Start-up parameters' page (attached) such as On-the-fly startup, Speed ramp duration, minimum start-up spee...
HI all I work with compressor, I use ST MotorControl Workbench to debug, after configuring and pressing start motor after, my compressor has no response.Can anyone help me? :folded_hands: :folded_hands: :folded_hands:
Hello, i've got trouble with receiving SPI in interrupt.Im running 2 SPI's on STM32F103RCT6; first is transmit only master, second is receive only slave, bus speed is 2MHz on both. SYSCLK is 64MHz.Transmitting works great (blocking mode), but HAL_SPI...
Hello,I'm using STM32CubeMX 6.3.0 with the bundled version of STM32CubeF4I create a new project by selecting my STM32F769I-DISCO board and letting Cube initialize all peripherals to their default modes. I generate the project into an SW4STM32 toolcha...
Hi,I have an ST25R3911B-DISCO and have discovered that UART and I2C are not supported on the loaded firmware through searching Google on how to use the interfaces.I am wondering if there have been any updates in the last two years on this subject.If ...
Kudos from