User Activity

Dear ST community, i don't know if any one encountered this issue before, however when i try to import the matplotlib module on the mickledore version of the openstlinux the system crushes like shown in here  Python 3.11.5 (main, 24 2024, 12:23:19) [...
Dear STM comunity, i am currently trying migrate my solution from the kirkstone to  mickledore because it offers more software functions that i need and cant properly use on the kirkstone, i have spent alot of time trying to port the configurations f...
Hello ST Dear ST Community, I'm currently trying to migrate my solution from stm32mp1-openstlinux-5-4-dunfell-mp1-20-06-24   to stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15 Im using a ST7789V Based LCD, and its working trough /dev/fb0 and ...
Dear ST community,I am currently trying to install an 8bit 8080 LCD , and i figured out that it needs FMC $ to be set up in devicetree in order to interface with it using DRM in Linux. i have the following device tree pinctrl nodes setup   fmc_pins_m...
i have been trying to use the LTDC peripheral on the Linux kernel to use it on the ILI9340 / ILI9340 in 8 bit mode.i use this in the device tree:  &ltdc { status = "okay"; port { #address-cells = <1>; #size-cells = <0>; ltdc_ep1_out: endpoi...
Kudos from
Kudos given to