Hi,how to differentiate both chips, if they have the same value for WHO_AM_I register?I know that I could read couple times the accelerometer values, calculate magnitude over all axis and check if the value is near 1g or 0.5g (assuming no movement du...
I wanted to try the STEVAL-IDP005V1 from STEVAL-BFA001V1B,I followed the description given in UM2438and nothing worked,Finally I realized that the cable description is wrong (or may be I've got a bad cable),the ground is on white, not on blue wire
Hello,how to order the STEVAL-MKSBOX1V1 to get current package content with JTAG adapter and cable?we ordered several pieces at Mouser and all of them are the old blisters without JTAG adapter and cablewe are also facing the battery won't charge / wo...
Hello Eleon,I made some further tests, after the configuration sucessfuly tested yesterday doesn't want to work on another desk today,the problem lays on some kind of interferences,the V2 is clocked just with 4MHz, the V3 with 24MHzso the default 4 M...
Hello Eleon BORLINI,not exactly, the DFU USB is working and JTAG is working when CPU is in DFU mode, but not when CPU is in normal mode.No, I cannot check with V2, because I do not have the adapter (see my other posts why),the V3 seems to be OK, beca...
Hello Eleon,a small update:it still does not work with newest FW I was able to find10:46:46:296 : ST-LINK FW : V3J7M2B4S1
10:46:46:298 : Voltage : 1.81V
10:46:46:298 : Error: No STM32 target found!it connects only when special mode entered (bootloade...