User Activity

The example from STM8L15x-16x-05x-AL31-L_StdPeriph_Lib doesn't explain the way a regular buffer (i.e. 20 - 30 bytes of data) exchange between two MCUs in master and slave mode. Can anyone explain the steps of configuration on both sides?Now I have ST...
Good day everyone.I'm trying to get Wiznet made W5500 working with STM32F030 series, using SPI in DMA mode.Unfortunately, in nSS hardware output mode, SPI bus pulls up nSS line after every transmitted byte (see attached image), while W5500 manual sta...