User Activity

Hy.I have a little problem. I developed an Ethernet based remote firmware update for the STM32H753 uC (rev. V) in a custom board.The processor erases the BANK2, and than programs it with the new firmware. When the programmed firmware checks correctly...
Posted on February 14, 2018 at 18:39Hy.I would like to download the crypto library. When I click the request software button, a form shows up. I fill the form correctly, but nothing happens, I cannot download the software.I really need the library. ...
Posted on February 11, 2017 at 20:39 Hy. I have a stm32f407vgt. I would like to use all TIM2 input compare for DMA trigger. I don't understand that the TIM2_CH4 is at two dma streams, and one of them with CH2, so how can i use all 4 channels at t...