I have the same problem with the dongle showing only 256KB and not 1MB. Nothing seems to load successfully.I used the stm32wb5x_FUS_fw.bin file that came with STM32Cube_FW_WB_V1.2.0. That loads OK. But, when loading co-processor firmware, it fails.I ...
Posted on February 04, 2017 at 18:52I don't have the schematic or layout in front of me, but inductors come in most of the standard sizes - certainly 0402 through 1206 - so finding a 0 ohm resistor of the same size is a matter of selecting the match...
Posted on February 03, 2017 at 19:47The 'L' designation does imply a inductor, however, an inductor might not be required at that point at this time, so a 0 ohm resistor is there to replace it and complete the RF circuit. At some later date, or in y...