Sgarr.1
Associate II
since
2020-06-15
2023-07-06
User statistics
3
Posts
0
Solutions
0
Kudos given
0
Kudos received
View all badges
STMicroelectronics Community
About Sgarr.1
Options
Report User
User Activity
Posts
Replies
No posts to display.
Re: Multiple vl53l1x sensor
2020-06-19
Hi jhon,i cant use this time 12 ms in the counting people application,use two sensor for the width of the door. Thanks El vie., 19 de junio de 2020 9:38 a. m., ST Community escribió:
Re: Multiple vl53l1x sensor
2020-06-18
hi, i am using the lidar 2d example, it works for me when i use only one sensor, but when i use two sensors it doesn't work, could you help me
Re: Multiple vl53l1x sensor
2020-06-18
hola, estoy usando el ejemplo de lidar 2d, funciona para mí cuando uso solo un sensor, pero cuando uso dos sensores no funciona, ¿podrían ayudarme?