Posted on September 22, 2017 at 14:58Hello, you're right both part-numbers are very similar (same Vbr range, same package,...). You can use both if your application respects the maximum values given in both datasheets. The better part-number is link...
Posted on January 11, 2017 at 09:26marking is the reference of circuit as colors marking gives the value for a resistor.You need which stress is applied on circuit and as defined in AN316 chapter 5, calculate the power dissipation for the TVS. See o...
Posted on January 11, 2017 at 09:22600 W peak power capability for 10/1000 us exponential waveform (rise time=10µs duration time (half of peak) = 1000 µs). All are described in AN316. Of course, over-voltages are not always in exponential waveform, ...
Posted on January 09, 2017 at 08:55All parameters in TVS datasheet are guaranteed without damage TVS (short-circuit or failure). TVS gola is to clamp (voltage limiting) over-votlages. If samsung requires 13.2 V, TVS Vrm has to be higher than 13.2 V ...
Posted on January 06, 2017 at 10:40Hello Andriy,We don't find any information with BUX marking code for TVS (ST or compet). So, for us, it's a mistake.If you want to reinforce the TVS robustness, we advice to use higher power capability: SMCJ12A (15...