We want to allow customers to download firmware directly.Are you trying to pass the STM32CubeProgrammer\bin file, no licensing issues?I'm trying to make a batch file so that I can download it right away.I've tested it. If you pass only this file and ...
Hello. We are working on a project that uses STM32H747 dual-core MCU.The ST-Link firmware is updated to the latest version, so debugging is not working well.So I'm going to lower it to the version I used before, but I can't download it. The lowest av...
Hello.We are working on a project that uses STM32H747 dual-core MCU.Debugging does not work well when downloading to the latest version.So I'm looking for the V2.J32.S7 firmware that I used before.Currently, the downloadable version is J36 or later.I...
hi~We are testing the motor development kit.MCU keeps dying at "steval-ctm010v1".220V in, RS232 cable is connected.The MCU dies when the debugger is connected.The debugger connection was not possible, so I connected the C82 capacitor NRST pin to the ...
You are about to enter the value of the motor parameter into the MotorControl Workbench.Do you know how to input the motor pole number, Rs, Ls, etc?The motor is intended to use the MSMF022L1S2 Panasonic motor.
We created a batch file and proceeded.The CLI file worked well only when the above files were present."(CLI.exe Program Location)\STM32_Programmer_CLI.exe" -c port=COM5 br=115200 P=EVEN db=8 sb=1 -w "(hex file location).hex"
I'm looking for easier documents, blogs, or videos.I want to easily run the development kit on the MotorControl Workbench.The development kit will arrive next week, and I don't think it'll be easy to operate just by looking at this document.