Posted on November 24, 2017 at 06:59 Looking at the https://community.st.com/servlet/JiveServlet/showImage/2-163506-19288/Capture.JPGfrom one of the comments above, I have made a truth table of BOOT0 state, Validity of Bank1 code and validity of ...
Posted on November 23, 2017 at 13:44Hey, I have a confusion regarding the BOOT0 configuration.Do I need to change the BOOT0 level from 0-> 1 or 1-> 0 to enter the bootloader mode? Or is it the case that, setting the BFB2 bit is same as setting the B...
Posted on November 23, 2017 at 13:20Hey CliveIs there any way to enter the bootloader mode without controlling the BOOT0 pin. In my application, there is only one microcontroller (STM32), and thus there is no way I can remotely control the BOOT0 pin...