Hello @JPabl.1,
Please make sure to use below versions of STM32 Tools and to respect default installation location.
STM32CubeProgrammer version 2.16.0 : STM32CubeProg - STM32CubeProgrammer software for all STM32 - STMicroelectronics
Please use ...
Hello @JPabl.1,
The X-TOUCHGFX-MPU Add-on is based on STM32Cube BareMetal Ecosystem.
There a getting started section in ST Wiki page which would help you to start your first TouchGFX project on STM32MP135F-DK board.
How to install X-TouchGFX MP...
Hi @JPabl.1,
There is no TouchGFX support on STM32 MPU devices running on OpenSTLinux (OSTL) distribution.
TouchGFX is being supported on STM32MP135 with BareMetal ecosystem (STM32Cube ecosystem not OSTL).
Please have a look on below ST Wiki pa...
Hello @DMårt,
Not sure to understand your query.
If your question is concerning the .NET package support within this distribution, then this is a different topic which I don't have answer :). Please feel free to start a new thread in the community an...
Hello @nesnes,
export QT_QPA_PLATFORM=wayland
If you would like to run your Qt application using the wayland backend then you likely need to switch to the weston user account.
Failed to create wl_display (No such file or directory)
otherwise the di...