User Activity

I'm working for the low power mode functionality on STM32H745ZI-Q ,it's dual core.I got perfectly sleep mode functionality on single interrupt that is PC13(EXTI_13).I done the functionality on M4 core....But I need the requirement like the SleepMode ...
Can you please help me anyone to solve the below warning as well as note in Ethernet configuration .....-->WARning ;-The ETH can work only when RAM is pointing at 0x24000000-->NOTE:-PHY Driver must be configured from the LwIP 'Platform Settings' top ...