User Activity

Hello!​​I am using b-l475e-iot01a1, and I am currently working on DAC using Timer and DMA.​DAC uses Ch1 of DAC1 and Timer uses TIM2.​The TRGO of TIM2 is Update Event, and the Trigger of DAC is using TIM2 Trigger Out Event.​Sine function values from 6...
I want to work on flash with B-L475E-IOT01A1.​After flash erase operation, flash write operation is performed, and memory is being checked through debugging.​On other boards, flash erase operation changed the memory in that location to the "?" mark, ...