User Activity

Hello,We are trying to make use of the ART accelerator of the STM32F7.As a start we placed only a single part of code in the adress range of 0x00200000.And we enabled the ART accelerator in CubeMx as well as code prefetch.However when we start the co...
Hello to all,We have to measure movements via an quadratur encoder.This is done via an external interupt that writes a timer capture to external memory.The old product used an STM32F2xxx with 120Mhz, the ISR was about 1us.However with the STM32F7 som...
Hi ST-Team,We want to use the STHS34PF80 for presence detection. I am not very familiar with the sensor, as a just watchedthe webinar about the sensor last Tuesday.I think a good way to check the capabilities of the sensor is the STM32 Open Developme...
Hello,I use CubeMX 6.1.0.Some peripherals I must initialize by myself for some reasons.So for example if I use the ADC1, I enable a dummy ADC peripheral in CubeMX AND I supress the code generation in ProjectManager/Advanced settings at the same time...
Hello to all,I am fighting for days now to get a simple Animated Image Example running on a new STM32F769I-EVAL Board Rev. BThe main problem is that the examples are downloaded from the cloud by the TouchGFX designer and are very very old!They do not...
Kudos from