Hello,XOSC_EN bit in Miscellaneous DCF helps for enabling the oscillator at device startup and the default configuration is with XOSC OFF. In your case I think you are just in one of the running modes the device supports. This is the common scenario ...
Dear Shambu,I understand you have the SPC58NG84E7QEH0Y in your hands.The additional feature I reported is for the other partnumber, not for the one you have.So this is why you don't know about the further information details.The special partnumber is...
Good afternoon Shambhu,with additional RAM we meant the possibility to use further memory for data storage other than the System RAM and Local RAM. The additional memory space is taken from peripheral and the list is available in the Technical Note.B...
Hello,the two parameters you need to satisfy for reliability and functionality are the ones passed in DS rev8 4.8.3."In order to ensure device reliability, the average current of the I/O on a single segmentshould remain below the IRMSSEG maximum valu...