Posted on February 05, 2013 at 09:24Correction: * Its INPUT middle level that shifts * the DAC divider has to be 1:2 so that it can cover full range from gain=1 to gain=16 Jurek
Posted on February 04, 2013 at 18:00OK i have a solution to this problem.To the useless trolls: The frequency response is not an issue because this op-amp has a rated bandwidth of 8MHz, so at gain=16 i still get over 100kHz (~500kHz?) usefull bandwi...
Posted on February 04, 2013 at 11:01Hello, I have the same problem with STM32F3, I have blocking-capacitor coupled signal on the non-inverting input, and the signal on the op-amp side is pulled to VDDA/2 by 50kOhm resistor. In other words, the signa...