User Activity

Now and again, following power-up, we find the STS1TX in our product in a state where we cannot interface with it. The SPI and GPIO lines are outputting ~2V levels, so no commands can be sent.Typically, cycling power may allow the chip to initialise ...
I am trying to configure the CR95HF (using either CR95HF.dll V0.9 or V1.2) to communicate with an M24SR02-Y, with an eventual view to read/writing NFC Forum Type 4 NDEF files. All I2C coding has been completed for "internal" access to the EEPROM/NDEF...
Posted on November 29, 2012 at 09:45I am trying to use DMA1 Stream 1 Channel 4 in the STM32F205ZE  (IAR Embedded Workbench IDE).   Attempts to configure the DMA (using the Std Peripherals library) result in no change in the register values (all val...
Kudos from