User Activity

Posted on September 27, 2012 at 18:35Does anybody know if the 96bit unique-ID has different fields? There's no much info about this unique ID (in the reference manual it is said that it has 96bits but after that, when the register is shown only the ...
Posted on September 27, 2012 at 11:21I am using STM32F405 in an application and in order to start working with the PWM module I have to check that I read a 100% duty cycle on one channel input. I've been reading documentation, but it seems that inp...